Part Number: INA241A
I am looking for a high voltage, precise current sense amplifier and both the INA241 and the INA296 families meet my design requirements. I see that the INA241 has a PWM reject feature like the INA750 and INA790. How do I decide…
Other Parts Discussed in Thread: C2000WARE
This thread will discuss the best practices for custom bootloading on the following devices:
F2807x
F2837xS
F2837xD
F28004x
F2838x
F28002x
F28003x
F280013x
F280015x
F28P65x
F28P55x …
Part Number: INA240
What Size Resistors should be used with the INA240?
Can a voltage divider be used to drive the reference input of the INA240?
Why does the output of the INA240 seem distorted compared to the measured current?
Part Number: TMCS1126
How do I calculate the Ioc and Voc thresholds?
What is the range of the overcurrent?
Is the overcurrent for both the positive and negative current?
Do you have a tool to calculate the Ioc and what value I need to apply on…
Other Parts Discussed in Thread: LM74502 , TPS272C45 Below is a list of all collateral pertaining to TI High Side Switch Devices (TPSxHxxx) devices. This includes TPSxHA, HB, HC, HCS devices.
Part Number: TMCS1123
Hi,
I would like to ask for clarification regarding the long-term insulation reliability of TMCS1123.
I have reviewed TI’s document High Frequency TDDB of Reinforced Isolation Dielectric Systems , which shows that, for polyimide…
Part Number: BQ25883
The BQ25883 and other devices in the family have a Soft Start Feature on Vsys output. This can be seen in datasheet fig77 that Vsys has a slow ramps-up. The Soft-Start feature at power up is noted in par 8.3.3.4.
Slow rate of…
Part Number: BQ25171-Q1 Other Parts Discussed in Thread: BQ25172 , BQ25173-Q1 , BQ25173 , , BQ25170
This home page is for common questions in relation to the BQ25171-Q1, BQ25173-Q1, BQ25170, BQ25172, BQ25173
FAQs
-------------------…
Part Number: MCF8329HS-Q1 Other Parts Discussed in Thread: MCF8329A , MCF8329HS
MCF8329HS: Advanced Motor Control IC with Enhanced Performance
The MCF8329HS builds upon the proven MCF8329A platform, delivering enhanced motor control capabilities and…