We're trying to source a 24.576 MHz crystal to use with the PCM1863. The datasheet appears to be silent on things like required tolerance, drift and ESR. Is that info available?
Thanks,
Scott
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
We're trying to source a 24.576 MHz crystal to use with the PCM1863. The datasheet appears to be silent on things like required tolerance, drift and ESR. Is that info available?
Thanks,
Scott
Hi Scott,
Unfortunately we don't have that info, but given the device has an internal PLL I think if you use a crystal that is spec'd under 100ppm tolerance you should be fine. That said, if you are running at a standard audio rate in slave mode then you don't actually need an SCKI as the device has an autoclock configuration feature and can generate internal clocks from BCLK.
Best,
Zak