This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TAS5733L: Questions about overvoltage and undervoltage

Part Number: TAS5733L

I configure ADR/FAULT as output to see if the chip is overvoltage or undervoltage. When I input 3.3V AVDD to the chip, ADR/FAULT displays as 1, and the chip is working normally, but when I input PVDD After 12V, ADR/FAULT has been switched between 0 and 1. Is this normal or an undervoltage and overvoltage fault has occurred? The PVDD input is 12V/200mA.