This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Product recommendation inquiry

Other Parts Discussed in Thread: TAS5721, TAS2770, TAS2564

Hi, TI Support Team

We request that you recommend a product that meets the spec below by adding a function to the car air purifier.

- Analog output: Stereo, 8W per ch (8ohm)

- EQ function

- Digital input: I2S

Please recommend a product that meets the above spec.

Thanks.

Regards,

MJ

  • Hello MJ, 

    Our team is looking into this thread and will respond as soon as possible. 

    Best Regards, 

    Justin Beigel

  • Hi MJ,

    Some options we could think of are TAS5721, TAS2770 or TAS2564.
    TAS2x devices are mono, TAS2564 has an integrated boost in case you need to supply the amplifier from some lower battery voltage.

    EQ would be the main concern as some of our devices with integrated DSP are rated for lower power. How much EQ functionalities are required?

    Best regards,
    -Ivan Salazar
    Applications Engineer - Low Power Audio & Actuators