Other Parts Discussed in Thread: TPA2016D2
Hi TI.
There's a question that customer wants to clarify.
They used TPA2017 along with AIC3101.
According to datasheet as below, Fixed Gain is 6dB, Max Gain is 30dB.
Questions are:
- Does it mean that Gain is 6 dB when AGC1,2 is set to 0,0?
- Is there a way to adjust the Amp Gain to Max 30 dB?
How do they use the amplifier?
Please answer to set different gain if default fixed gain is limited to 6dB.