The datasheet says that this device has a built-in "short circuit protection circuit".
Please teach us about this function.
In the description of the datasheet
・When a short circuit is detected in the output, the shutter down mode is set.
・Shutdown mode can be canceled by changing the SHUTDOWN pin from low to high, or by turning the electric power from OFF to ON.
-If the short circuit is not released, it will be shut down again.
It has been described as.
The current circuit "SHUTDOWN pin is fixed high".
In this state
(1)When the output (ROUTP and ROUTN) is short-circuited
"Short circuit detection-> shutdown mode-> shutdown mode cancellation-> short circuit detection ..."
Will short circuit detection and shutdown mode be repeated?
Or is it still in shutdown mode because the "SHUTDOWN pin change from low to high" is not detected?
* The power remains ON.
(2) When ROUTP and ROUTN are short-circuited and the shutdown mode is set, is it okay to recognize that the output of the L side output (LOUTR, LOUT) is also stopped?
(3) In the case of "short circuit detection and shutdown mode are repeated", is there any effect on the device (heat generation, damage in some cases, ignition, etc.)?
(4) When a signal is input to the signal pins (LIN, RIN) in shutdown mode, is there any effect on the device?
(5) The R side output (ROUTP and ROUTN) is short-circuited, but the speaker connected to the L side is producing sound.
It seems that the short circuit protection is not working, but is there any effect on the device when using it in this state?
* The R side input (RINN) is a variable resistor with no input signal (input voltage 0V).
It is unconfirmed whether the input voltage is completely 0V.
Or is it just not noticed because the short circuit protection function is working but the "short circuit detection and shutdown mode" repeats quickly?
For the circuit, refer to "Figure 17" on page 15 of the data sheet.
* Since the speaker is connected to an 8Ω product,
"L1, L2 = 33uH, C1 = 0.47uF, C2, C3 = 0.1uF"
It is supposed to be.
I think the questions are duplicated, but thank you.