Part Number: PCM2912A
Other Parts Discussed in Thread: PCM2912
Hi
Could you help check the PCM2912 schematic as below and any need to adjust
Thanks
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
1. I see 2 identical circuits of PCM2912 With Identical nets. Why is this so?
2. A single Ground Plane is fine for the circuit.
You can provide 3.3v/6Mhz clock to XTI pin. XTO can be left open. Use a 22 ohm resistor in series with source producing 6Mhz