This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TAS5780M: How to initialize the IC using a .cfg file

Part Number: TAS5780M
Other Parts Discussed in Thread: , TAS5825M, TAS5754M

I am trying to use PurePath Console 3 to create a .cfg file that I can use to initialize the TAS5780M amplifier on our product.  I started with the TAS5780MEVM.  I can initialize the EVM using PPC3 (with the Audio Processing block), and the amplifier IC outputs are switching as expected.  If I write out a .cfg file of that configuration using the End System Integration block, power cycle the EVM, and then reload the saved .cfg file using the Direct I2C block, all the writes happen but the amplifier IC outputs are not switching.  It seems like there is something missing in the .cfg file.

Is there something else I have to do after loading the .cfg file to get the amplifier to start?

Thank you!

-Dan