This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TLV320AIC3254: AIC3254 AGC Configuration for Silence Detection

Part Number: TLV320AIC3254

Hi 

We use Luis Fernando Rodríguez S's script to verify the silent detection function via INT1, it works.

We have some questions about AGC configuration need your help:

1.  We only need the silent detection function, and we hope that the original input signal will not be  affected by the AGC feature. Do you have any suggestion AGC configuration for us?

2. Regard the AGC interrupt feature, we observed that it seems only trigger interrupt when the signal power was lower than Noise Threshold. 

Our question is :

If we got an interrupt(signal power was lower than Noise Threshold) , then when the ambient noise increases(Signal power is greater than Noise Threshold), is there any method to let us know about this event.

Thanks.

BR

Trevor