I have access to PP3, and the TAS2110EVM App. All are installed, and I can connect and read/write from the device.
The jumpers on the EVM are set to the default internal. I'm connected to a bench power supply, 5V 3A.
I've tried multiple speakers, both 4 ohm. No matter what I try, when I select TI USB Audio UAC2.0 as my output device, I get nothing. Sound works properly using other playback devices.
I've tried to play with some of the settings in the control app, but nothing there seems like it would prevent it from working. I followed the User Guide, with the exception of the device sample rate. That window doesn't exist in Windows 10 as far as I can tell.
Thoughts? Any help is appreciated.