This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPA3111D1: Fault and Shutdown Pin connection

Part Number: TPA3111D1

Hi Team,

As per EVK if we connect Fault and Shutdown Pin together it will allow amplifier to self-reset after short-circuit protection event. In this case do we required any MCU GPIO connection with this pins ?

We have limitation of GPIO so is it mandatory to connect any MCU GPIO with Fault and Shutdown Pin ?

We just want to tie Shutdown and Fault pin together and no additional GPIO of MCU. Will it work ? 

  • Hi,

    SD and Fault pin connected together without GPIO is fine. You should add pull-up on SD pin to make device start up properly.

    Connecting to MCU will let MCU know there is fault happened on TPA3111.

    Regards,

    Derek