Other Parts Discussed in Thread: , TAS5414A, TPA6404-Q1
Hello,
My customer is asking about TAS5414C at PBLTL mode(mono).
1) Can TAS5414C output with following connection?
Conditions:
DC supply(PVDD): 12V、
Speaker: load 1Ω(0.8Ω min.)
Output : 60W Max
2) In PBLTL mode(mono), which OUT N/P is connected to speaker’s polarity?
Out1 N/P or Out3 N/P -> Speaker + ?
Out2 N/P or Out4 N/P -> Speaker - ?
PBTL mode connection isn’t described in datasheet..
Regards,
Tao_2199