Other Parts Discussed in Thread: TAS6422Q1EVM,
Hello, the audio transmission rate is limited to 48khz (in 16 and 24 bits) on the TAS6422EQ1VM (XMOS) and on the TAS6422Q1EVM (TAS1020)
In optical input the limit is also 48kHz. If I send audio at 88.2 or higher, the card fails and no sound comes out. If I go back to 48kHz, even without erasing the fault, the sound works again.
I can't find "If sampling frequency is greater than 48 kHz, select 96 kHz from the “Input FS” pull down." as explained in the instructions (in PPCC app).
Thank you in advance.