This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TAS5622A: Input two voltage

Part Number: TAS5622A

Hi Team,

If I change the input voltage of the tweeter to 12V,
The input voltage of the subwoofer is 24V,
Is there a problem with the circuit?