Other Parts Discussed in Thread: TAS6424E-Q1
Dears,
Consult tas6424-q1 or tas6424e-q1 Whether it can support 2 Ω load when PvdD = 25V power supply in Po_BTL mode (connect the seat vibrator in a planned way, and the DC impedance range of the seat vibrator is 2 ± 20% Ω; the minimum value is 1.6 Ω; refer to the impedance curve as follows:)
For other speakers (driven by independent power amplifier channel), the minimum impedance of the speaker is 2.88 Ω according to its error range; In this state, whether the chip works normally. If not, what risks may there be? Thank you!