READY signal:
What does READY do? Tas5630.pdf (also called SLES220B) does not really say. The only
clues are in the PIN FUNCTIONS table statement ‘Normal operation; open drain; active high’ and a hint that
it has something to do with overcurrent detection in SYSTEM DESIGN
CONFIGURATION. So what is abnormal operation? Why does the signal name appear as
active-low (with an over-bar) in tables on pages 4 and
11? How is READY related to the warning signals (/OTW, /SD for DKD package, and /OTW1, /OTW2, /SD, /CLIP for PHD package) and /RESET?
/RESET signal (see tas5630.pdf page 24):
In DEVICE RESET, tas5630.pdf says ‘Asserting reset input
low removes any fault information to be signaled on the SD output, i.e., SD is
forced high. A rising-edge transition on reset input allows the device to resume
operation after an overload fault. To ensure thermal reliability, the rising
edge of reset must occur no sooner than 4 ms after the falling edge of SD.’ I assume this means /SD latches but will go high (with what delay?) after /RESET goes low, and /RESET should stay low at least 4 ms after /SD goes high. Please clarify.
In SYSTEM DESIGN CONFIGURATION, tas5630.pdf says ‘Apply only audio when the state of READY is high that will start and stop the amplifier without having audibleartifacts that is heard in the output transducers. If an overcurrent protection event is introduced the READY signal goes low, hence, filtering is needed if the signal is intended for audio muting in non microcontroller systems.’ This statement is very unclear. Should 'Apply only' be 'Only apply'? Should 'that is heard' be 'that are heard'? Is there supposed to a period separating 'high' and 'that' to make two sentences? What signal is to be filtered, and how would a filter prevent an overcurrent event latch? Please clarify.
In PIN-TO-PIN SHORT PROTECTION, tas5630.pdf says ‘To make sure the PPSC detection system is not tripped, it is recommended not to insert resistive load to GND_X or PVDD_X’. My breadboard circuit has about 28.8K ohms to ground from each of the two PBTL outputs. There is about 3mA internal pull-down current (Ipd on page 11) from each half-bridge during reset, so I have assumed that another 0.85mA will not foul operations. Please verify.
OLPC (Overload protection counter) : What does it do?
Overcurrent response time : I assume 'flip-state' refers to setting a latch. Please clarify.