This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPA3255: Maximum load on DDV HTSSOP package

Part Number: TPA3255

Hello,

There are several discussion on E2E about maximum load weigh on DDV HTSSOP package for Heatsink attachment.

What is your package development team characterization result to secure lifetime reliability for "no package clack and no die de-lamination" ?

 

Is there application note DDV HTSSOP usage guide?  Long time ago I have seen such a document.

Which is correct maximum load number 90N or 100N?

Do we need to apply 50% guard band on mass production assembly?

 

Regards,

Mochizuki