This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TAS5622A: Wattage difference between TAS5622A and TAS5342LA

Part Number: TAS5622A
Other Parts Discussed in Thread: TAS5342LA

Hi Team,

For the same 1 watt output condition, the input PWM level is different,

is the circuit of the two devices the same?

are there any differences in the datasheets of the two devices?

  1. TAS5622A 180.9mV measured 1W
  2. TAS5342LA 378mV measured 1W