Hi team,
Our customer have a question about the PCM6360-Q1.
The Input Line in is the 1kHz signal source, and the output is output disconnected.
As the pictures shown, the yellow is output and the green is input.
The content of the attachment is the register configuration of PAGE0.
Why does this happen?
[ 137.075881] REG:0x1:0x0 [ 137.076197] REG:0x2:0x1 [ 137.076465] REG:0x3:0x0 [ 137.076727] REG:0x4:0x0 [ 137.076996] REG:0x5:0x5 [ 137.077244] REG:0x6:0x0 [ 137.077568] REG:0x7:0x34 [ 137.077832] REG:0x8:0x0 [ 137.078177] REG:0x9:0x0 [ 137.078616] REG:0xa:0x0 [ 137.079077] REG:0xb:0x0 [ 137.079422] REG:0xc:0x1 [ 137.079683] REG:0xd:0x2 [ 137.079953] REG:0xe:0x3 [ 137.080232] REG:0xf:0x4 [ 137.080524] REG:0x10:0x5 [ 137.080776] REG:0x11:0x6 [ 137.081061] REG:0x12:0x7 [ 137.081412] REG:0x13:0x2 [ 137.081735] REG:0x14:0x48 [ 137.082522] REG:0x15:0x48 [ 137.082963] REG:0x16:0x10 [ 137.083566] REG:0x17:0x10 [ 137.084000] REG:0x18:0x4 [ 137.084344] REG:0x19:0x20 [ 137.084609] REG:0x1a:0x2 [ 137.084838] REG:0x1b:0x8 [ 137.085113] REG:0x1c:0x0 [ 137.085350] REG:0x1d:0x0 [ 137.085591] REG:0x1e:0x2 [ 137.085841] REG:0x1f:0x40 [ 137.086072] REG:0x20:0x0 [ 137.086313] REG:0x21:0x22 [ 137.086529] REG:0x22:0x0 [ 137.086732] REG:0x23:0x0 [ 137.086933] REG:0x24:0x0 [ 137.087134] REG:0x25:0x0 [ 137.087338] REG:0x26:0x0 [ 137.087575] REG:0x27:0x0 [ 137.087779] REG:0x28:0x10 [ 137.087984] REG:0x29:0xff [ 137.088196] REG:0x2a:0x3 [ 137.088402] REG:0x2b:0x0 [ 137.088609] REG:0x2c:0xc0 [ 137.088813] REG:0x2d:0xc [ 137.089026] REG:0x2e:0x0 [ 137.089231] REG:0x2f:0x0 [ 137.089444] REG:0x30:0x0 [ 137.089649] REG:0x31:0x0 [ 137.089852] REG:0x32:0x8 [ 137.090092] REG:0x33:0x8 [ 137.090299] REG:0x34:0x0 [ 137.090575] REG:0x35:0x0 [ 137.090805] REG:0x36:0x0 [ 137.091018] REG:0x37:0x40 [ 137.091223] REG:0x38:0xba [ 137.091449] REG:0x39:0x4b [ 137.091696] REG:0x3a:0x10 [ 137.091941] REG:0x3b:0x70 [ 137.092227] REG:0x3c:0x98 [ 137.092565] REG:0x3d:0x0 [ 137.092794] REG:0x3e:0xc9 [ 137.093000] REG:0x3f:0x80 [ 137.093203] REG:0x40:0x0 [ 137.093408] REG:0x41:0x98 [ 137.093613] REG:0x42:0x0 [ 137.093818] REG:0x43:0xc9 [ 137.094024] REG:0x44:0x80 [ 137.094228] REG:0x45:0x0 [ 137.094425] REG:0x46:0xb8 [ 137.094665] REG:0x47:0x0 [ 137.095034] REG:0x48:0xc9 [ 137.095267] REG:0x49:0x80 [ 137.095565] REG:0x4a:0x0 [ 137.095849] REG:0x4b:0xb8 [ 137.096284] REG:0x4c:0x0 [ 137.096516] REG:0x4d:0xc9 [ 137.096745] REG:0x4e:0x80 [ 137.097031] REG:0x4f:0x0 [ 137.097293] REG:0x50:0x38 [ 137.097563] REG:0x51:0x0 [ 137.097818] REG:0x52:0xc9 [ 137.098054] REG:0x53:0x80 [ 137.098292] REG:0x54:0x0 [ 137.098586] REG:0x55:0x38 [ 137.098917] REG:0x56:0x0 [ 137.099292] REG:0x57:0xc9 [ 137.099593] REG:0x58:0x80 [ 137.099913] REG:0x59:0x0 [ 137.100314] REG:0x5a:0x0 [ 137.100684] REG:0x5b:0x0 [ 137.101071] REG:0x5c:0xc9 [ 137.101536] REG:0x5d:0x80 [ 137.101955] REG:0x5e:0x0 [ 137.102244] REG:0x5f:0x0 [ 137.102540] REG:0x60:0x0 [ 137.102815] REG:0x61:0xc9 [ 137.103080] REG:0x62:0x80 [ 137.103344] REG:0x63:0x0 [ 137.103625] REG:0x64:0x3c [ 137.103889] REG:0x65:0x37 [ 137.104192] REG:0x66:0x7f [ 137.104480] REG:0x67:0xb8 [ 137.104750] REG:0x68:0x0 [ 137.105014] REG:0x69:0x0 [ 137.105282] REG:0x6a:0x0 [ 137.105549] REG:0x6b:0x1 [ 137.105815] REG:0x6c:0x48 [ 137.106082] REG:0x6d:0x7b [ 137.106346] REG:0x6e:0x0 [ 137.106639] REG:0x6f:0x0 [ 137.106942] REG:0x70:0xe7 [ 137.107217] REG:0x71:0x0 [ 137.107487] REG:0x72:0x0 [ 137.107755] REG:0x73:0xfc [ 137.108080] REG:0x74:0xfc [ 137.108398] REG:0x75:0xe8 [ 137.108658] REG:0x76:0xf0 [ 137.108919] REG:0x77:0xec [ 137.109180] REG:0x78:0x0 [ 137.109445] REG:0x79:0x0
Thanks.
Best Regards,
Xiaoxiang Liu