Other Parts Discussed in Thread: TLV320AIC3120
The icons in the init script dialog are not enabled/ highlighted after connecting the EVM to the PC via USB.
Please suggest me the solution.
Thanks in advance.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
The icons in the init script dialog are not enabled/ highlighted after connecting the EVM to the PC via USB.
Please suggest me the solution.
Thanks in advance.
Hi,
Apologies for the delay, please wait at least 12-24 hours for our codec expert to respond to your question.
Thank you for your patience.
Hi,
If the icon is not highlighted that means it's not available for this device, but you can click the view tab and select entry like the init script which configure the device directly.
Regards.
Hi,
I need another help. I am connecting aux cable from PC to CODEC evaluation board (TLV320AIC3120) and playing song from PC. When MICLP was connected to DAC mixer. I am able to listen the song via speaker and headphone.
So now I wanted to know, how to prove the path which was hightlighted below in red. Is there any way to record the audio which was fed to mic as record option not highlighted for TLV320AIC3120 EVM and any other looopback options available is also fine.
Yes you can use tool like Audacity or GoldWave to record incoming audio through USB.
Good.