This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi,
Please help recommend a 20W audio amplifier, the requirements are as follows:
1. Support PBTL and BTL modes;
2. 12V power supply, can support up to 15W/CH@4Ω power output in BTL mode, no requirement for THD+N
3. The PA efficiency is above 90%
4. GAIN is not less than 32dB
Best Regards
Charlie Xiao
Hi Charlie,
These requirements would need a Class-D or similar amplifier. Moving this post to the group that covers these devices.
Regards,
Mike
Hi Charlie.
Base on your requirement, you can choose amps like below:
Digital input AMP: TAS5805M/TAS5825M
Analog input AMP: TPA3129D2/TPA3116D2
You can choose other chips that you think are better through our official website.
Speaker amps product selection | TI.com
BR.
Wei Qiu.