Other Parts Discussed in Thread: DS90UB949-Q1, PCM1753, PCM1754
Hi,
We are configuring DAC using spi master device. Spi configurations are as below:
1. spi mode0 is used(CPOL=0, CPOH = 0)
2. spi speed 1Mbps
3. Data Tx width 16 bit
4. data mode LSB first
we are configuring register 20 as below settings.

Below is the spi data traced at our end. Please verify data is going to dac in correct format or not.

Also check input waveforms BCK, DATA, LRCK and SCK using logic analyzer. We have given SCK of 33MHz from PLL. sampling rate is 44.1KHz, multiple of 768fs.

Please verify the output waveforms at left and right channel. we are getting noise on right channel and noise plus audio at left channel.


Regards,
Mohit