This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Dear Sirs,
I have a question.
The description of Zero Detect condition on page 16 of the data sheet is as follows.
If the data for a given channel remains at a 0 level for 1024 sample periods (or LRCK clock periods), a zero-detect condition exists for that channel.
Is the output of the DAC muted in this condition?
Please let me know above question.
Best Regards,
Y,Hasebe
Hi, Hasebe-san,
Zero detect function of the PCM1753 does not mute the output of the DAC. When a zero is detected, the device will indicate the event with a Zero flag according to the channel where the zero data has been detected (ZEROR[pin11] or ZEROL[pin12]). These flags can be used to operate external circuitry used to to mute the DAC.
Best Regards,
-Diego Meléndez López
Audio Applications Engineer
Hello Diego-san,
Thank you for your quickly and kindness reply.
I understand your comments.
Then I have one more question.
Although I understood about ZeroDetect, DAC is not output when input data changes to without input data.
In this case I think that the output of the DAC is stopped internally.
Is it correct?
Best Regards,
Y.Hasebe