HI!
I use the With PBTL Output and Single-Ended Input mode. In the TPA3110D2, after a logical "1" is applied to the SD input, the sound appears at the output of the microcircuit with a delay of more than 300ms. When using the same circuit and with the same parameters in TPA3110LD2, the delay is minimal, about 15ms. It has been tested on dozens of different series of microcircuits, from different suppliers, experiments have been carried out for a long time. What do you advise?