This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
I'm currently considering a control method to automatically increase the volume of low-pressure sounds.Is there anything that can be done with purepath console3's GUI settings?
The amplifier I am using is "TAS5806".
Thank you for your support.
Ishibashi Takeru
Hi Ishibashi
you can set the automatically volume increase of low-pressure sounds by use DRC function at PPC3. Select the region and set the ratio with your actual application. for example shown as this picture:
Thank you for your reply.
Is there a setting to automatically normalize high and low sound pressures in an audio signal?
For example, in a web conference, the voices of the participants may be loud or soft, and the volume of these voices should be automatically adjusted to the same level.
Ishibashi Takeru
Hi Ishibashi
It need use MIC to record the voice and match algorithm, we don't have this program
I understand. thank you.
I think "DRC" and "Equalizer/FIR Filter" are similar, but what is the difference?
Ishibashi Takeru
Hi Ishibashi
the "DRC" and "EQ" is not same, the DRC setting work while signal trigger the threshold, but the EQ setting work whether or not the threshold is triggered