Measurements of a TAS5630DKD2EVM show that no-load usable output voltage in PBTL mode is limited to about 29.4Vrms with a 50VDC power supply or 28.1Vrms with a 48VDC power supply. Those are where the output waveforms start to have noise bursts at their high and/or low peaks. Some older and not quite comparable measurements of a TAS5615 EVM, indicate it would output about 2Vrms more. Do these figures seem typical?
Would using output filters (15uH, 0.68uF) like those in the TAS5615 EVM reduce modulation noise to increase the usable output voltage, maybe to the level that the TAS5615 EVM delivered? I don't need all of the power that a TAS5630 can deliver but I do need as much output voltage as possible.