Greetings,
I made a board with the TPA3110D2, and it presents a high level of constant white noise hiss. If I short the input to GND, the noise disappears, but I'm not sure what to do to reduce the noise level. I've tried the board connecting it to a motherboard, and supplying it power from the same source. If the power comes from a different adapter than the motherboard, the noise is significantly reduced. The gain is set to 20dB
I also tried a board with the same IC that I bought on Ebay to compare its performance, and the noise level is quite lower, even if powered by the same source as the motherboard. This board had the power limiter set at half the VGDD, but I tried removing the power limit (connecting PLIMIT to GVDD) and the noise level is still lower than that of my board.
These are the schematics/PCB of my board. Is there anything on the input side that might be the cause of the poor performance?
Thank you kindly,