This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TAS6424L-Q1: There is 100k clutter in the output.

Part Number: TAS6424L-Q1


Hi team,

For TDM, when the customer is playing 1kHz audio, he finds that there is clutter around 100kHz superimposed on the output waveform. At this time, the fault is that the audio is playing and the audio is not playing. I hope BU can help to find out whether this signal is related to DSP or power amplifier 6424L?

OUTPUT:RED AND BLUE

SCLK:YELLOW

SDIN:PINK