Dear ladies and gentleman,
I'm trying for quiet a time now to get a TAS3204 DSP working and after some discarded pcb layouts I finally produced a layout with low noise and a working TAS3204. Or at least I believe that the TAS is working since the I/O test configuration streams audio through the DSP. The problem is that I can't persuade the TAS to follow an EEProm programming. My biggest problem is to figure out, where the failure is located. On a oszillioscope I can see a datatransfer between the EEProm and the TAS, but that's about it. I have attached my test configuration from the pure path studio hoping, that you could check it and maybe try to program it into a TAS3204 to see if this part is correctly done so far.
Greeting from Germany
Christopher