Other Parts Discussed in Thread: TLV320AIC3104
I have setup the audio codec as described within 'TLV320AIC3104 Programming Made Easy', and the differential outputs clip when LOP/M output-control set >= 6dB. For our power, AVDD, DRVDD, and IOVDD are powered by 3.3V, and DVDD is powered by 1.8V. We are using the following register settings, which primarily follow 'TLV320AIC3104 Programming Made Easy'.
Why, with standard settings, are the outputs clipped when the amplifier is set >= 6dB?
Also, when set to 0dB, I only get 3.7V peak-peak, and I believe that this should be closer to 4.0V per the data sheet. Why would that be?
I have attached screenshots of both 0dB and 9dB.