Please check the Rjc(top) is 0.4°C/W or 0.7°C/W of TAS6424MS-Q1.
It's 0.4°C/W in 7.4 Thermal Information but 0.7°C/W in Table 12-1 of tis Datasheet.
Thank you
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Please check the Rjc(top) is 0.4°C/W or 0.7°C/W of TAS6424MS-Q1.
It's 0.4°C/W in 7.4 Thermal Information but 0.7°C/W in Table 12-1 of tis Datasheet.
Thank you
The specifications located in table 7.4 are correct. You should be using the value of 1.1-C/W for your calculations.
Regards,
Gregg Scott
So do you mean I should using the value of 1.1°C/W not 0.4 °C/W when simulation modeling with a heatsink?
Thanks