This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Dear
PCM3168A is configured as a TDM8 output, and the LRCKAD and LRCKDA are combined to connect to the LRCK of the main control chip
After BCKAD and BCKDA are merged, BCKAD is connected to BCK=12.288M of the main control chip, SPI mode of the main control, PCM3168 as slave, sampling rate LRCK:48K MCLK: 12.88M, BCK: 12.288M;
addr=42, val=0
addr=43, val=0
addr=44, val=0
addr=45, val=0
addr=46, val=0
addr=47, val=ff
addr=48, val=ff
addr=49, val=ff
addr=4a, val=ff
addr=4b, val=ff
addr=4c, val=ff
addr=4d, val=ff
addr=4e, val=ff
addr=4f, val=ff
addr=50, val=1
addr=51, val=6
addr=52, val=0
addr=53, val=0
addr=54, val=0
addr=55, val=0
addr=56, val=0
addr=57, val=0
addr=58, val=d7
addr=59, val=d7
addr=5a, val=d7
addr=5b, val=d7
addr=5c, val=d7
addr=5d, val=d7
addr=5e, val=d7
---readback---:
addr=c0, val=c0
addr=c1, val=6
addr=c2, val=0
addr=c3, val=0
addr=c4, val=0
addr=c5, val=ff
addr=c6, val=0
addr=c7, val=ff
addr=c8, val=ff
addr=c9, val=ff
addr=ca, val=ff
addr=cb, val=ff
addr=cc, val=ff
addr=cd, val=ff
addr=ce, val=ff
addr=cf, val=ff
addr=d0, val=1
addr=d1, val=6
addr=d2, val=0
addr=d3, val=0
addr=d4, val=0
addr=d5, val=0
addr=d6, val=0
addr=d7, val=0
addr=d8, val=d7
addr=d9, val=d7
addr=da, val=d7
addr=db, val=d7
addr=dc, val=d7
addr=dd, val=d7
addr=de, val=d7
The output of 48K slave mode of TDM8 is normal. After the sampling rate is 96K, the output of single rate, double rate and automatic rate is abnormal. Please help to check the configuration of the 96K which needs to be changed, thank you! When configured in dua rate or auto mode, ADC DATA does not generate waveform; when configured in single rate, there is noise
Hello Liu,
When reviewing the registers above I have noticed the following:
After the sampling rate is 96K, the output of single rate, double rate and automatic rate is abnormal.
Let me know if this helps.
Best,
Andrew
hi andrew ,
Thank you for your reply,
1) Register addr=45, val=0 #no flags, reply :This is because no signal comes out from ADC, so no signal is sent to DAC, indicating that 0 is detected
2) Current configuration
MCLK=BCLK=24.5M ,addr=40, val= c2.addr =50, val=2 are all set to dual-rate mode .The problem now is that the clock is working properly, that is, the ADC has no data output, and the ADC is always low ,See Waveform and log information
.PCM3168 Init...
.write:
.addr=40, val=c2
.addr=41, val=6
.addr=42, val=0
.addr=43, val=0
.addr=44, val=0
.addr=45, val=0
.addr=46, val=0
.addr=47, val=ff
.addr=48, val=ff
.addr=49, val=ff
.addr=4a, val=ff
.addr=4b, val=ff
.addr=4c, val=ff
.addr=4d, val=ff
.addr=4e, val=ff
.addr=4f, val=ff
.addr=50, val=2
.addr=51, val=6
.addr=52, val=0
.addr=53, val=0
.addr=54, val=0
.addr=55, val=0
.addr=56, val=0
.addr=57, val=0
.addr=58, val=d7
.addr=59, val=d7
.addr=5a, val=d7
.addr=5b, val=d7
.addr=5c, val=d7
.addr=5d, val=d7
addr=5e, val=d7
---readback---:
.addr=c0, val=c2
.addr=c1, val=6
.addr=c2, val=0
.addr=c3, val=0
.addr=c4, val=0
.addr=c5, val=ff
.addr=c6, val=0
.addr=c7, val=ff
.addr=c8, val=ff
.addr=c9, val=ff
.addr=ca, val=ff
.addr=cb, val=ff
.addr=cc, val=ff
.addr=cd, val=ff
.addr=ce, val=ff
.addr=cf, val=ff
.addr=d0, val=2
.addr=d1, val=6
.addr=d2, val=0
.addr=d3, val=0
.addr=d4, val=0
.addr=d5, val=0
.addr=d6, val=0
.addr=d7, val=0
.addr=d8, val=d7
.addr=d9, val=d7
.addr=da, val=d7
addr=db, val=d7
addr=dc, val=d7
.addr=dd, val=d7
.addr=de, val=d7
.
.---PCM3168 Init OK---!
.
.time2=344
.
.......i2sout underflow 476
.uart_data_process......
.datas in nvram
.Please press 'ENTER to enter into console,then type 'help' for help
[dsp] Init_DSP_Para OK
[dsp] time=331
.[dsp] in:0.000000, 0.000000, 0.000000, 0.000000
.[dsp] out:0.000000, 0.000000, 0.000000, 0.000000
Hi Liu,
If the master device is not providing valid BCLK to the PCM3168, then there will be no valid I2S output from the device. The BCLK needs to be a square wave from 0V - DVDD with a duty cycle of around 50%.
Can you improve the clock input's quality? Also, what is your scope bandwidth?
Best,
Andrew
hi Andrew It is 100MHz bandwidth ,You mean the BCLK clock is not like a square wave ? Let me retest bclk , Is there a problem with the register configuration ?
Liu,
A 100MHz Bandwidth scope is good. I was checking to see of it was a scope limitation. Causing a bad BCLK wave form (Please check the frequency rating of your scope probes as well).
The register configuration look okay. The capture from your previous post, however, shows BCLK as a 'triangle' shape. It also looks like this waveform goes from 1V-2V and this is not a valid BCLK. This means that there is either an issue with BCLK or the scope (or probes) is not acquiring the signal correctly).
Making sure BCLK is a square wave that goes from 0V to the DVDD rail is the next step in the debug process.
Best,
Andrew
Hi Liu,
PCM3168 does not have a compatibility issue. To understand what is happening in your application we first need to ensure that the BCLK is valid.
Currently, the BCLK given to the device is not a valid wave form since it does not go low (to 0V). Data will not output without a BCLK. Please provide the PCM3168 with a BCLK that actually provides a logic high and a logic low, then we can proceed with the debug process.
Best,
Andrew
Hi Liu,
I see no immediate issues with the schematic. Do you have any results from applying a valid bit clock?
Best,
Andrw
hi Andrew
The clock is generated by DSP , I cannot to changed. Why is the 48K TDM8 OK?
Hi Liu,
If I had to guess, the DSP is able to provide a valid BCLK when operating at 48k. To confirm this please capture wave forms (like the ones above) of the clocks at 48k sample rate.
Best,
Andrew
Hello again Liu,
Before following my previous post please see the below datasheet table. s
From my understanding, your desired setting should be as follows:
Based on your screen shot in previous posts it looks like the BCLK is ~24MHz which would be too fast for this configuration. However, the SCKI (MCLK) input still needs to be 24.576MHz.
I apologize if this was misleading in previous posts, I should have clarified earlier.
Best,
Andrew
Hi Andrew
I know you mean, DAC works in High speed mode and only needs one data, but ADC does not have high speed mode, so DIN 1\2 is needed for 96K, but my DSP does not have two data pins. Do you any way to make ADC work in high speed mode ? only need a data wire ?
Hi Liu,
Highspeed mode is not available for the ADC. In order to operate both the ADC and the DAC on the same dateline then, the sample rate would have to be decreased to 48kHz.
However, using two Data lines a 96k sample rate is possible.
Best,
Andrew
thanks Andrew,
The DSP does not support the input of two data cables D0\D1 . thank you very much for your support.