This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TAS6424M-Q1: PBTL mode

Part Number: TAS6424M-Q1
Other Parts Discussed in Thread: TAS6424, TAS6424E

We are considering using the TAS6424M-Q1 in PBTL mode with a 1ohm load.

We refer to "Figure 82. TAS6424M-Q1 Typical 2-Channel PBTL Application Schematic" in the Datasheet.

The output current of the amplifier will be higher than 4ohm because of the 1ohm load condition.

One of the problems is that the current balance may not be equal at the two output terminals of the same channel due to variations in specifications such as the inductor value and DCR value of the output coils used in PBTL mode.

 Example: Relationship between OUT_1P (pin 34) and OUT_1M (pin 32) and between OUT_2P (pin 40) and OUT_2M (pin 38)

In this case, does the TAS6424M-Q1 have a problem with current imbalance?

Or does it have to maintain a moderate current balance to maintain stable operation and electrical characteristics?

We would like some advice.

Generally, for normal BTL, we use a 2-in-1 output coil and design it for push/pull operation to minimize variation.

We would appreciate your opinion.