Hi team,
My customer has trouble of noise clipping(cracked) when playing back sound recorded with the TLV320AIC3120's microphone input.
They consider to adjust following register setting for recording.
Is there any suggestion for recommended setting for these registers or any other register which should be optimized?
=======================
Table 7-117. Page 0 / Register 86 (0x56): AGC Control 1 - p100
Table 7-118. Page 0 / Register 87 (0x57): AGC Control 2 - p100
Table 7-119. Page 0 / Register 88 (0x58): AGC Maximum Gain - p101
Table 7-120. Page 0 / Register 89 (0x59): AGC Attack Time - p101
Table 7-121. Page 0 / Register 90 (0x5A): AGC Decay Time - p101
Table 7-122. Page 0 / Register 91 (0x5B): AGC Noise Debounce - p101
Table 7-122. Page 0 / Register 91 (0x5B): AGC Noise Debounce (continued) - p102
Table 7-123. Page 0 / Register 92 (0x5C): AGC Signal Debounce - p102
Table 7-124. Page 0 / Register 93 (0x5D): AGC Gain-Applied Reading - p102
Table 7-161. Page-4 Registers - p111
Table 7-161. Page-4 Registers (continued) - p112
Table 7-161. Page-4 Registers (continued) - p113
Table 7-161. Page-4 Registers (continued) - p114
=======================
Best regards,
Shota Mago