This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

PCM1808EVM: Distorted signal

Part Number: PCM1808EVM
Other Parts Discussed in Thread: PCM1808

Hi,

I'm testing the PCM1808EVM evaluation board. I have to use the device as a slave device so I set up the board in slave mode, put MD0 and MD1 to GND.
I generate a SCKI clock signal using a PWM signal from the microcontroller (ESP32S3) at 8 Mhz so the audio sample rate is 31250 Hz. The clock rise and fall times seems within spec...
When recording a 1 kHz sine wave, the digitalized signal is distorted heavily.

Could someone look at my clock measurements here and suggest any possible solutions/options to make this device work in slave mode?

Thanks!

CH1 (yellow) = SCKI
CH2 (blue) = BCK
CH3 (magenta) = LRCK