Other Parts Discussed in Thread: PCM1808,
Hi,
The datasheet states that a single-ended voltage input of 3 Vpp is allowed. The absolute ratings for the analog input voltage V_in_L, V_in_R are stated as follows:
Minimum: -0.3 V
Maximum: (VCC + 0.3 V) < 6.5
Does this mean I need to make sure my input audio signal is always abov3 -0.3V?
When I have for example a 3 Vpp audio signal do I need to DC offset it by +1.5 V so it alternates between 0 and +3 V instead of alternating between -1.5 V and +1.5 V?
Thanks