Hi,
I'm using the TAS5630DKD with PSU rails at 40VDC. Power requirements are low at 90W/ch in 4ohms.
Implementation is very similar to the evaluation board, but due to severe space limitations I had to use a smaller inductor that I saw mentioned elsewhere on the TI forum for a TAS5613, the Coiltronics CTX10-2-52-R (10uH ,4.7A). Capacitors are Panasonic ECW-F2684JAQ (680nF 250V MKP)
Even though they do work and I managed to push a fair amount of power through them, plus the output waveforms look OK.
Unfortunately, the inductors get scorchingly hot, as in >70degrees Celsius without ANY input signal or output load.
Any help would be appreciated.