Other Parts Discussed in Thread: TLV320AIC3120
Hello,
We have a working prototype using this part. All of the clocking settings are unchanged from how the default init script on the EVM sets them. We are driving this speaker from the Class-D outputs: https://www.visaton.de/sites/default/files/dd_product/k50_8.pdf and are hearing distortion. The speaker is rated for 2 watts which is higher than the TLV320 datasheet says the Class-D amps can deliver into an 8 ohm speaker (1.6W). Any help would be appreciated. Thanks.