Hi Ivan,
I am again working on a script with Adaptive Filtering, using the EVM as start point.
While checking everything, I discovered the following lines on the command interface:
(this will be added to the command interface when I program the device for the use of the Adaptive Filtering Feature)
w 30 00 2C 04
w 30 00 2C
w 30 0C 00 00 00 00 0A BE 8D 00 00 00 00 00 00 00 00 00 00 00 00 00
here,
w 30 00 2C 04
The script seems to change to Page 44, but then adds '04' which is a Reserved register (?)
The DAC3203 would then go into Auto Increment mode, but it has nothing to write into the register,
because the script changes again into page 44:
w 30 00 2C
and now, yes, writes into the corresponding registers
w 30 0C 00 00 00 00 0A BE 8D 00 00 00 00 00 00 00 00 00 00 00 00 00
Am I missing something here?
Anyway, the DAC3203 seems to catch this and works fine, but I want to be sure, not to add any potential bug into the code.
Thanks for the help and best regards,
Gustavo