We have run into an unusual problem with the TAS5806MD amplifier. We have two amplifier ICs on our PCB. One is set up for 2.0 BTL, and the other for 1.0 PBTL. Both amplifiers seem to take the initialization from the .cfg files created by PurePath properly. But, in some cases, there is a deep notch at 6 kHz that isn't programmed in the filters (in fact, we are not using any audio processing in the amplifier, so the response should be completely flat). Not all amplifier PCBAs exhibit this problem all the time and some exhibit the problem more than others. To confirm the audio we are sending to the amplifier was not the issue, we put a DAC in parallel with one of the amplifier ICs, and the amplifier output had the deep notch at 6 kHz but the DAC output was flat. Some amplifier ICs reproduce the 6 kHz notch almost every time. Others show it only sporadically after repeated power cycles.
We tried to reproduce this on the TAS5806MD EVM, but were unable to do so. We then used a logic analyzer to capture the I2C traffic between PurePath and the EVM, and the data does not line up with what is in the .cfg file created by PurePath for the same project file. There appear to be a lot of other commands to the amplifier in addition to what is in the .cfg files (we ignored the I2C traffic to other devices, which we presume to be other peripheral ICs on the EVM). This makes us wonder if there is something missing in the .cfg file that is needed to make the amplifier work as it does on the EVM.
Has anyone else seen this deep notch at 6 kHz? Is there something we are doing (or not doing) during the initialization of the amplifier that could cause this problem? Is this a known issue with this amplifier IC?
Thank you!
-Dan