Hi I'm Jieun,
I have some questions about TLV320AIC3120 Audio CODEC.
In datasheet, it indicates that the recommended level of inputs is 0.707Vrms(@AVDD=3.3V, single-ended).
I was wondering if I could know Line input and Line output voltage level ranges(min~max) for under the below cases.
when AVDD=3.3V, single-ended line input & output
when AVDD=3.3V, differential line input & output
when AVDD=1.8V, single-ended line input & output
when AVDD=1.8V, differential line input & output
best regards,