Hi team,
Consists of a combination of L-channel...no signal and R-channel...audio signal
Stereo signals are input to pin 14 (SDIN) of the TAS5825P as serial data and output from pin 23 (OUT_B+) and pin 27 (OUT_B-) as R-channel signals.
Should the unused pins 2 (OUT_A+) and 30 (OUT_A-) be connected to pins 1 (BST_A+) and 29 (BST_A-) via capacitors, respectively?
Also, should a load resistor be connected to pins 2 (OUT_A+) and 30 (OUT_A-) that are not used?
If you have any other recommendations for use, we would appreciate it if you could provide them.
Best,
Ryu.