We are using the TAS5713 digital audio amplifier in a product. The chip is configured in PBTL mode for a single channel audio output. We have working product/firmware and just completed a pre-production build of 110 boards. During production test of the boards, we discovered > 10% of the boards have a very annoying "click" at the startup of audio playback. This click is independent of the volume control setting. We have played with the settings for the STOP/START PERIOD REGISTER and all this does is delay the time to when the click is heard when starting up the audio. I suspect this relates to taking the part out of shutdown mode. All boards were tested with the same speaker attached to rule out this being an off-board hardware problem. Anyone seen similar problems with this part?
Thanks,
Dave