Other Parts Discussed in Thread: TAS5719
Dear,
One customer used TAS5719EM to test the SNR, he tested the output noise floor of headphone higher than 110uV, SNR is 83dB.
The test condition is as this:
1. Connected external 12V regulator to power the EVM board, 5V regulator to power the headphone.
2. First connected the ADC of motherboard, audio signal external to TAS5719, configure TAS5719 by I2C, the headphone output is normal. Then connected the I2S_DATA to GND, test the noise floor of headphone, it is higher than 11uVrms.
3. The gain of the headphone is 0dB and 6dB, the output noise floor is the same.
So he couldn't get the goal of the datasheet.
Do we have any other data about the EVM test?
Best regards
Kailyn