This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TAS6422-Q1: DC Load Diagnostic: About Open load Detection

Part Number: TAS6422-Q1

Hi TI Support Team,

The configuration of the amplifier remains default setting for all register so it begins PLAY mode for two channel.are active and used load is 4 ohm speaker. I read only 0x0C register for the aim. Let's consider 2 cases for open load detection:

CASE 1:

At the beginning the load is not connected to CH1 and the second load is connected CH2. Energized and then  It can be monitored CH1 OL:Open load detected, CH2 OL: No Open load detected. After connecting the load to CH1, CH1 OL:No Open load detected. This CASE is OK.  

CASE 2: 

Both speakers are connected to the channels. After energizied the compenent,When I remove the one of the speakers in ANY TIME, It can not be monitored the OL states properly. The amplifier is continiued to report No open Load detected for both channel. I mean the DC  Open load detection is working correctly for once at the beginnig but it doesn't work properly instantaneously. For detecting instantaneously should I use AC Load diagostic or is there any   way?  is there any API or libraries of the amplifier for the application software? 

By the way I can not understand what Channel state DC diagnostics mode in 0x04 was. I tried the bit fields as changing to DC load Diagnostic and then read register 0x0C. But It didn't work :). 

  • Hi 

     Both DC and AC diag can't be used during PLAY state. Your testing results are correct. Only Real Time Load Diag could detect load status during PLAY, but this device doesn't have this feature. 

    By the way I can not understand what Channel state DC diagnostics mode in 0x04 was.

    Try it during Hi-Z state, and could consider try it with open load, then check 0x0C status. The normal load diag only takes 260ms and finished. Only when there's a fault, will keep in this status.

  • "Both DC and AC diag can't be used during PLAY state. Your testing results are correct. Only Real Time Load Diag could detect load status during PLAY, but this device doesn't have this feature." Thank you so much this info and feedback. 

    "Try it during Hi-Z state, and could consider try it with open load, then check 0x0C status. ."

    For you said above I tried the steps below:

    1. Check the channel states from  the register 0x0F.

    2. If one of them is Hi-Z, set the DC Load diag to the channel which is Hi-Z from the register 0x04..

    3. Read  and monitor the diagnostic load states in 0x0C.

    But it runs like in CASE 2. I couldn't understand that If the device has not the feature real time open load detection, it already can not be find the channel state in any time, too. Am I wrong?. Can you explain in detail above that you said?

  • Hi 

    it already can not be find the channel state in any time, too. Am I wrong?. Can you explain in detail above that you said?

    If the device already into PLAY state, and open load appears, then indeed there's no way for the device to detect it. Only the open load condition happens before device PLAY, could be detected.

    But if it is short circuit, the OC protection would take effect, and device reprot FAULT. Then even you try to reset the device or clear the fault, the DC Load Diag will take effect, and detected there's still short ciruit, it won't back into PLAY.

  • Hi,

    But if it is short circuit, the OC protection would take effect, and device reprot FAULT. Then even you try to reset the device or clear the fault, the DC Load Diag will take effect, and detected there's still short ciruit, it won't back into PLAY.

    Yes, I have obtained the similar results for the short circuit. If the device is begin to run whose the load is shorted to GND, Amplifier is reported that it was shorted to GND. After the removed the jumper between GND and the load, it iwas run in PLAY and reported No Shorted to GND. But If it is begin to run in PLAY and normally, It could not be detect it even if I have shorted it to GND later and then didn't back to  PLAY.

    I only tried AC diagnostic mode for open load detection. But it wasn't useful and effective because it has to be change channel state to Hi-Z and need to operate out of  its functionality itself even if I use the its sound as a test signal. 

    Thanks a lot your feedback.

  • Hi 

    AC load diag is specially for tweeter, or capacitor coupled load, when DC diag will find open load for these speakers. It's not very easy to use, need to give a high frequency signal, and use register value to calculate the impedance value.

  • Yes I could test and read some impedance values of the load both when it was connected and when it was not  as follwing the step in the datasheet. (using the sound itself  for experimental purposes. the sound is very complex, whose the frequency band is wide.).  

    Acc. to thedatasheet, "When the test is complete the channel reporting register indicates the status change from the AC diagnostic
    mode to the Hi-Z state. The detected impedance is stored in the appropriate I2C register." So I waited to change of the CH state and then read the impedance. But it takes a time a bit ,It stays in MUTE until the changing the CH state That's why I don't find it practical term as its functionality.

    Thanks a lot your all responses and for taking the time. Although I cannot perform real-time open load detection or any DC diagnostic etc., I now recognize the component."