Hi,
I designed a Power Amplifier which used TAS5611 and it works very well. The bulk capacitor that I used is 1000uF, because both the EVM and Schematic of datasheet use 1000uF capacitor. In my case, the input signal has high peak to average ratio, and the frequency is from 14kHz to 20kHz. So, Is it possible to reduce the capacitance of the bulk capacitor? How to compute this capacitance? I looked some documents that talked about the bulk computation issue. Is the bulk capacitance have linear relationship with 1/Fin, Fin is the input signal frequency. Thanks
Regards
Xiaoka