This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

OPA1656: The lowest noise and highest SNR configuration.

Part Number: OPA1656
Other Parts Discussed in Thread: JFE2140, , OPA202, INA849, JFE150EVM, JFE2140EVM, JFE150, OPA145

Hi,

I want to know the proper configuration to connect a low-frequency antenna (L = 12mH @ Rdc = 7.5Ω @ Cp = ~ 60pF)  to an opa1656 amplifier with a required gain of around 200~300 and a bandwidth of approximately 3kHz - 300kHz, while minimizing noise, is needed to add entry level such us JFET JFE2140?

Best Regards.