This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TAS6424E-Q1: TAS6424E-Q1 Spread Spectrum Issue

Part Number: TAS6424E-Q1
Other Parts Discussed in Thread: TAS6424E,

Tool/software:

(1) Am I correct in understanding that spread-spectrum is enabled not only at 2.1MHz but also at 480KHz and 384KHz PWM frequencies?
(2) Will the calculation formulas also change for 480KHz and 384KHz? Especially the calculation of SS_PRE_DIV.
(3) The SS frequency TYP value of 8% is listed in the performance section, but what is the limit value?

I would like to add to your question,
In (2) below, if the formula remains the same, please tell me what happens to the factor “11” at 2.1MHz at 480KHz.
If the formula remains the same, please tell me how the factor of “11” at 2.1MHz would be at 480KHz.

In (3) below, the 8% deviation range mentioned means that Fmin varies in the range from Fcent to (1-8%) x Fcent with respect to Fcent.
Is it correct to say that Fmin varies in the range from Fcent to (1-8%) x Fcent?