Other Parts Discussed in Thread: TAS6422-Q1
Tool/software:
Hi Team,
We are using the TAS6422QDKQRQ1 in our design for the product.
Following are the Amplifier configuration done through I2C
1. Mode Control Register 0x00 = 0x00 -> BTL mode
2. SAP Control (Serial Audio-Port Control) Register 0x03 = 0x04 -> I2S 16-bit (sine Wave Data transfer from the Controller)
3. Channel State Control Register 0x04 = 0x05 -> play Mode
4. Channel 1 Through 2 Volume Control Registers 0x05 and 0x06 = 0xCF ->0dB
5. DC Load Diagnostic Control 2 Register 0x0A = 0x77 -> we are using 4Ohm Speaker.
WE aslo measured the All the I2S Clock , which are as expected with following value
1. MCLK - 24 MHz
2. BCLK - 3 MHz
3. SYNC - 44 kHz
4. TXD - -- Sine wave data.
Issue:
Always we are hearing some unknown tone in the speaker. Even the MCLK is not available.
Can you check and suggest the I2C setting is correct?
Our application schematic is same as Figure 77. Typical 2-Channel BTL Application Schematic (TAS6422-Q1.pdf).