TPA3131D2: Fault keep high/ low cycle change during start up

Part Number: TPA3131D2

Tool/software:

Hi expert,

Customer recently face to random no audio output issue after power up in MP project.

The project is mass production for a long time, and recently have two boards don't have audio output.

We have measured fault pin and find fault pin is in low<-> high cycle. We have checked the failed condition which may trigger to fault, but there are no short circuit/ over current/ DC offset/ etc. fault. Also find an e2e post which talking about input cap quality, we test it and measured the waveform but no failed been found.

The fault pin will keep high(have audio output) after system run in window and then change sound volume. 

Since we only have two failed board on hand. Before do ABA swap test. Any waveform measurement we can do to verify issue root cause?

Regards,

Ben